Fixing mode:
By the body
Movement of operating head:
Rotary
Type of operator:
Spring return without operating lever
Type of approach:
Lateral approach, 2 directions
Type of operator Type of operator:
Spring return without operating lever
Type of approach Type of approach:
Lateral approach
Operator direction information:
2 directions
Narrow by