应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
left right
Navigation Remove all  
应用
Common Characteristics  
输出信号类型: 离散
电气连接
电气连接: 1 针型接头
Narrow by
 
Products 1 to 2 of 2
 Per page  |   1 
Configuration option
XU5M18U1D thumbnails - Schneider-electric XU5M18U1D
光电开关,漫射式
Is not part of a configuration
Obsolete reference cannot be added to the basket
XURU1KSMM12 thumbnails - Schneider-electric XURU1KSMM12
光电开关,颜色检测
Is not part of a configuration
Obsolete reference cannot be added to the basket