应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
left right
Navigation Remove all  
应用
 
Products 1 to 1 of 2 (Total: 1)
 Per page  |   1 
Configuration option
XUYAFLCO966S thumbnails - Schneider-electric XUYAFLCO966S
DINEL光亮传感器
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYDCFPCO966S thumbnails - Schneider-electric XUYDCFPCO966S
Is not part of a configuration
Add to basket