应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
left right
Navigation Remove all  
应用
 
Products 1 to 9 of 10 (Total: 9)
 Per page  |   1 
Configuration option
XURZ01 thumbnails - Schneider-electric XURZ01
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XURZ02 thumbnails - Schneider-electric XURZ02
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYFPDC101
DINEL色标传感器光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYFPDC61
DINEL色标传感器光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYFPDCM8101
DINEL色标传感器光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYFPDCM861
DINEL色标传感器光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYA005
DINEL塑料光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYA110 thumbnails - Schneider-electric XUYA110
DINEL ECOFIBER概念塑料光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUYA310 thumbnails - Schneider-electric XUYA310
DINEL ECOFIBER概念塑料光纤
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUZC50HP thumbnails - Schneider-electric XUZC50HP
Is not part of a configuration
Add to basket