应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
Long distance or semi opaque object detection product offer consists of
 "High excess" gain sensor
 Fixing and mounting accessories as fixing brackets…..
 Cabling accessories consist of connectors and pre-wired connectors
left right
Navigation Remove all  
应用
Narrow by
 
Products 1 to 5 of 5
 Per page  |   1 
Configuration option
XUZA218 thumbnails - Schneider-electric XUZA218
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUZ2001 thumbnails - Schneider-electric XUZ2001
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUZ2003 thumbnails - Schneider-electric XUZ2003
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUZA118 thumbnails - Schneider-electric XUZA118
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket
XUZB2003 thumbnails - Schneider-electric XUZB2003
光电开关附件
Is not part of a configuration
Obsolete reference cannot be added to the basket