应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
Long distance or semi opaque object detection product offer consists of
 "High excess" gain sensor
 Fixing and mounting accessories as fixing brackets…..
 Cabling accessories consist of connectors and pre-wired connectors
left right
Navigation Remove all  
应用
Common Characteristics  
附件/独立安装部件类型: "连接器"
电气连接
连接器类型: M12
插脚数: 4 针
Narrow by
 
Products 1 to 5 of 5
 Per page  |   1 
Configuration option
XZCC12FCM40B thumbnails - Schneider-electric XZCC12FCM40B
接头
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCC12FCP40B thumbnails - Schneider-electric XZCC12FCP40B
接头
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCC12FCP42B thumbnails - Schneider-electric XZCC12FCP42B
接头
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCC12FDM40B thumbnails - Schneider-electric XZCC12FDM40B
接头
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCC12FDP40B thumbnails - Schneider-electric XZCC12FDP40B
接头
Is not part of a configuration
Obsolete reference cannot be added to the basket