应用
minus Hide
OsiSense XU Application offer is the answer to definite needs as
Detection in food & beverage sector with IP69K stainless steel housing sensors
Detection of transparency material
Detection of colour mark
Detection of invisible mark (luminescence)
Detection of colour
Detection integrated into the rollers conveyors systems
Distance measurement and precise positionning
Detection of illumination
Detection on long distance or semi opaque object with high excess gain sensor
Detection of water (aqueous liquid)
Detection offer dedicated to tertiary sector
RollerSensor offer consists of
Photo-electric sensors directly integrated into the rollers conveyors systems
left right
Navigation Remove all  
应用
Narrow by
 
Products 1 to 4 of 5 (Total: 4)
 Per page  |   1 
Configuration option
XZCR1511041C1 thumbnails - Schneider-electric XZCR1511041C1
跳线电缆
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCR1511041C2 thumbnails - Schneider-electric XZCR1511041C2
跳线电缆
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCR1512041C1 thumbnails - Schneider-electric XZCR1512041C1
跳线电缆
Is not part of a configuration
Obsolete reference cannot be added to the basket
XZCR1512041C2 thumbnails - Schneider-electric XZCR1512041C2
跳线电缆
Is not part of a configuration
Obsolete reference cannot be added to the basket
QO140M200I thumbnails - Schneider-electric QO140M200I
Is not part of a configuration
Add to basket