Navigation Remove all  
L100 / L300 Severe Duty Mill and Foundry with extended contact sequences
Narrow by
 
Products 1 to 20 of 49
 Per page  |   1   2   3  >
Product availability
HL100WDL2M7 thumbnails - Schneider-electric HL100WDL2M7
L100 mill limit switch - 2 contacts - spring return - CCW - 1/2" NPT
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WDL2M8 thumbnails - Schneider-electric HL100WDL2M8
L100 mill limit switch - 2 contacts - spring return - CW - 1/2" NPT
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WDR2M4 thumbnails - Schneider-electric HL100WDR2M4
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WDR2M5 thumbnails - Schneider-electric HL100WDR2M5
L100 mill limit switch - 2 contacts - spring return - CCW - 1/2" NPT
Obsolete reference cannot be added to the basket
HL100WS2M1 thumbnails - Schneider-electric HL100WS2M1
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WS2M2 thumbnails - Schneider-electric HL100WS2M2
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WS2M3 thumbnails - Schneider-electric HL100WS2M3
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WTL2M13 thumbnails - Schneider-electric HL100WTL2M13
L100 mill limit switch - 3 contacts - spring return - CCW - 3/4" NPT
Obsolete reference cannot be added to the basket
HL100WTR2M10 thumbnails - Schneider-electric HL100WTR2M10
L100 mill limit switch - 3 contacts - spring return - CW - 3/4" NPT
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL100WTR2M11 thumbnails - Schneider-electric HL100WTR2M11
L100 mill limit switch - 3 contacts - spring return - CCW - 3/4" NPT
Obsolete reference cannot be added to the basket
HL300WDL2M7 thumbnails - Schneider-electric HL300WDL2M7
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WDL2M8 thumbnails - Schneider-electric HL300WDL2M8
L300 foundry limit switch - 2 contacts - spring return - CW - 1/2" NPT
Obsolete reference cannot be added to the basket
HL300WDR2M4 thumbnails - Schneider-electric HL300WDR2M4
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WDR2M5 thumbnails - Schneider-electric HL300WDR2M5
L300 foundry limit switch - 2 contacts - spring return - CCW - 1/2" NPT
Obsolete reference cannot be added to the basket
HL300WS2M1 thumbnails - Schneider-electric HL300WS2M1
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WS2M2 thumbnails - Schneider-electric HL300WS2M2
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WS2M3 thumbnails - Schneider-electric HL300WS2M3
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WTL2M13 thumbnails - Schneider-electric HL300WTL2M13
L300 foundry limit switch - 3 contacts - spring return - CCW - 3/4" NPT
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WTL2M14 thumbnails - Schneider-electric HL300WTL2M14
LIMIT SWITCH
Non-Stock - Not normally stocked in distribution facility
Add to basket
HL300WTR2M10 thumbnails - Schneider-electric HL300WTR2M10
L300 foundry limit switch - 3 contacts - spring return - CW - 3/4" NPT
Non-Stock - Not normally stocked in distribution facility
Add to basket