|
|
|
HL100WN2M17
Limit switch, L100/300, L100 mill 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL100WNC2M18
Limit switch, L100/300, L100 mill 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL100WNCS2M34
L100 mill limit switch - 2 contacts - spring return - CW+CCW - 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL100WNSL2M29
L100 mill limit switch - 2 contacts - spring return - CW+CCW - 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL100WTLN1C2M39
Limit switch, L100/300, L100 mill 3 contacts, spring return, CW+CCW, 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
HL100WTRN1C2M38
L100 mill limit switch - 3 contacts - spring return - CW+CCW - 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
HL300WN2M17
Limit switch, L100/300, L300 foundry 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL300WNC2M18
Limit switch, L100/300, L300 foundry 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL300WNSL2M29
Limit switch, L100/300, L300 foundry 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
HL300WTLN1C2M39
L300 foundry limit switch - 3 contacts - spring return - CW+CCW - 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
HL300WTRN1C2M38
L300 foundry limit switch - 3 contacts - spring return - CW+CCW - 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
L300WN2M17
Limit switch, L100/300, L300 foundry 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
L300WNSL2M29
Limit switch, L100/300, L300 foundry 2 contacts, spring return, CW+CCW, 1/2" NPT
|
Is not part of a configuration
|
|
|
|
|
L300WTLN1C2M39
L300 foundry limit switch - 3 contacts - spring return - CW+CCW - 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
L300WTRN1C2M38
Limit switch, L100/300, L300 foundry 3 contacts, spring return, CW+CCW, 3/4" NPT
|
Is not part of a configuration
|
|
|
|
|
ML100WN2M16
L100 mill limit switch - 2 contacts - spring return - CW+CCW - M20
|
Is not part of a configuration
|
|
|
|
|
ML100WN2M17
L100 mill limit switch - 2 contacts - spring return - CW+CCW - M20
|
Is not part of a configuration
|
|
|
|
|
ML100WNC2M18
L100 mill limit switch - 2 contacts - spring return - CW+CCW - M20
|
Is not part of a configuration
|
|
|
|
|
ML100WNCS2M34
L100 mill limit switch - 2 contacts - spring return - CW+CCW - M20
|
Is not part of a configuration
|
|
|
|
|
ML100WNS2M26
L100 mill limit switch - 2 contacts - spring return - CW+CCW - M20
|
Is not part of a configuration
|
|