This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Környezetvédelmi közzététel
PEP-Thalassa PLA
English
2024-04-30
Brosúra
Műanyag és üvegszál erősítésű poliészter szekrények brosúra
Hungarian
2024-04-15
Megfelelőségi nyilatkozat
NSYPAPLA57G EU RoHS nyilatkozat
Hungarian
2024-04-02
NSYPAPLA57G EU RoHS nyilatkozat
Belső ajtó PLA szekrényhez (500*750)
NSYPAPLA57G Kínai RoHS nyilatkozat
Hungarian
2024-04-02
NSYPAPLA57G Kínai RoHS nyilatkozat
Belső ajtó PLA szekrényhez (500*750)
NSYPAPLA57G REACh nyilatkozat
Hungarian
2024-04-02
NSYPAPLA57G REACh nyilatkozat
Belső ajtó PLA szekrényhez (500*750)
Használati útmutató adatlap
Instruction Shett - Thalassa PLA - Internal Door
SILENT
2024-04-15
CAD
Thalassa PLA - 7035 inner door for 500x750 PLA - 3D CAD