This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
CAE
Spacial S3D CAE package for EPLAN
SILENT
2024-04-15
Környezetvédelmi közzététel
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-04-30
Megfelelőségi nyilatkozat
NSYPIN128 EU RoHS nyilatkozat
Hungarian
2024-05-07
NSYPIN128 EU RoHS nyilatkozat
Belső ajtó (1200*800)
NSYPIN128 Kínai RoHS nyilatkozat
Hungarian
2024-05-07
NSYPIN128 Kínai RoHS nyilatkozat
Belső ajtó (1200*800)
NSYPIN128 REACh nyilatkozat
Hungarian
2024-05-07
NSYPIN128 REACh nyilatkozat
Belső ajtó (1200*800)
Felhasználói kézikönyv
User manual for Spacial CRN(G) INNER DOOR
SILENT
2024-04-15
CAD
Spacial S3D CRN S3X - H1200xW800 - Internal door - 3D CAD