This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Környezetvédelmi közzététel
UE_Spacial SF, Steel floor-standing enclosure
English
2024-06-15
Használati útmutató adatlap
Spacial SF / Spacial SM - 19" swing racks - Instruction Sheet