This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Környezetvédelmi közzététel
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Megfelelőségi nyilatkozat
NSYSMVR18 EU RoHS nyilatkozat
Hungarian
2024-04-02
NSYSMVR18 EU RoHS nyilatkozat
2 függőleges adaptációs profil 1800
NSYSMVR18 Kínai RoHS nyilatkozat
Hungarian
2024-04-02
NSYSMVR18 Kínai RoHS nyilatkozat
2 függőleges adaptációs profil 1800
NSYSMVR18 REACh nyilatkozat
Hungarian
2024-04-02
NSYSMVR18 REACh nyilatkozat
2 függőleges adaptációs profil 1800
CAD
Spacial SM - 2 vertical adapt profiles 1800 - 3D CAD