Navigation Remove all  
9007 T/FT Severe Duty Mill and Foundry Limit Switches
Narrow by
 
Products 1 to 17 of 17
 Per page  |   1 
Configuration option
9007FTSB2M11 thumbnails - Schneider-electric 9007FTSB2M11
9007FT foundry limit switch - standard - spring return - CW+CCW - M20
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTSB2M12 thumbnails - Schneider-electric 9007FTSB2M12
9007FT foundry limit switch - standard - spring return - CW+CCW - PG 13.5
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTUB2M11 thumbnails - Schneider-electric 9007FTUB2M11
Limit switch, 9007, 9007FT foundry universal, spring return, CW only, M20
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTUB2M12 thumbnails - Schneider-electric 9007FTUB2M12
9007FT foundry limit switch - universal - spring return - CW only - PG 13.5
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TSB2M11 thumbnails - Schneider-electric 9007TSB2M11
9007T mill limit switch - standard - spring return - CW+CCW - M20
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TSB2M12 thumbnails - Schneider-electric 9007TSB2M12
9007T mill limit switch - standard - spring return - CW+CCW - PG 13.5
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TUB2M11 thumbnails - Schneider-electric 9007TUB2M11
Limit switch, 9007, 9007FT mill universal, spring return, CW only, M20
Is not part of a configuration
Add to basket
9007TUB2M12 thumbnails - Schneider-electric 9007TUB2M12
Limit switch, 9007, 9007FT mill universal, spring return, CW only, PG 13.5
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTSB2 thumbnails - Schneider-electric 9007FTSB2
Limit switch, 9007, 9007FT foundry standard, spring return, CW+CCW, 1/2" NPT
Is not part of a configuration
Add to basket
9007TSB2 thumbnails - Schneider-electric 9007TSB2
9007T mill limit switch - standard - spring return - CW+CCW - 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTUB2 thumbnails - Schneider-electric 9007FTUB2
Limit switch, 9007, 9007FT foundry universal, spring return, CW only, 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TUB2 thumbnails - Schneider-electric 9007TUB2
Limit switch, 9007, 9007FT mill universal, spring return, CW only, 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTUB6
9007FT foundry limit switch - universal - spring return - CCW only - 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007FTUB6M11
Limit switch, 9007, 9007FT foundry universal, spring return, CCW only, M20
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TUB6
Limit switch, 9007, 600 VAC 30amp t +options
Is not part of a configuration
Add to basket
9007TUD2
Limit switch, 9007, 9007FT mill universal, spring return, CW only, 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket
9007TUD6
Limit switch, 9007, 9007FT mill universal, spring return, CCW, 1/2" NPT
Is not part of a configuration
Obsolete reference cannot be added to the basket