Navigation Remove all  
L525 belt conveyor switches without lever
Common Characteristics  
Type of roller
Type of roller: Lateral roller
Number of circuits: 1
Diameter: 31.75 mm
Narrow by
 
Products 1 to 3 of 3
 Per page  |   1 
Configuration option
AL1650 thumbnails - Schneider-electric AL1650
Limit switch lever, L525, operating
Is not part of a configuration
Add to basket
AL16501 thumbnails - Schneider-electric AL16501
Limit switch lever, L525, operating
Is not part of a configuration
Add to basket
AL1802 thumbnails - Schneider-electric AL1802
LEVER OPERATING
Is not part of a configuration
Obsolete reference cannot be added to the basket