Navigation Remove all  
L140 / L2153 rope pull switches
Common Characteristics  
Type of operator
Type of operator: Stay put lever for cable attachment
Material: Aluminium
Narrow by
 
Products 1 to 5 of 5
 Per page  |   1 
Configuration option
AL1649 thumbnails - Schneider-electric AL1649
Limit switch lever, L2153, stop, aluminum, fixed length, for AL1746
Is not part of a configuration
Add to basket
AL1746 thumbnails - Schneider-electric AL1746
LEVER OPERATING
Is not part of a configuration
Obsolete reference cannot be added to the basket
KA thumbnails - Schneider-electric KA
Limit switch lever, L140, cable pull 1.5 emergency stop
Is not part of a configuration
Add to basket
KB thumbnails - Schneider-electric KB
LEVER CABLE PULL 3 EMERGENCY STOP
Is not part of a configuration
Obsolete reference cannot be added to the basket
KO thumbnails - Schneider-electric KO
LEVER CABLE PULL 2.5 EMERGENCY STOP
Is not part of a configuration
Obsolete reference cannot be added to the basket